MX50: Precaution when using SPI in slave mode -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX50: Precaution when using SPI in slave mode -blog archive

897 Views
PeterChan
NXP Employee
NXP Employee

If you have read the IMX50 chip errata, you may note that there are several issues related to the eCSPI and CSPI in slave mode. Do not attempt to transmit data more than the BURST_LENGTH. The SPI will continue to consume your TX data buffer after BURST_LENGTH is reached it will transmit corrupted data when BURST_LENGTH is crossed.

 

 

Tags (1)
0 Kudos
Reply
0 Replies