MX28: force system to boot in recovery mode -blog archive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX28: force system to boot in recovery mode -blog archive

1,122件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Typically, to boot the MX28 system in recovery mode, end user should hold the recovery switch for several seconds while plugging in USB. Alternatively, the system can set the real time clock persistent bit HW_RTC_PERSISTENT1:0x8005C070:0 and then execute system reboot. Detail can refer to "Boot Modes" section in  reference manual.

Once the MX28 is in recovery mode, PC host can load any MX28 boot stream to the device using sb_loader.exe via USB.

タグ(1)
0 件の賞賛
返信
0 返答(返信)