MX28: force system to boot in recovery mode -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX28: force system to boot in recovery mode -blog archive

789 Views
PeterChan
NXP Employee
NXP Employee

Typically, to boot the MX28 system in recovery mode, end user should hold the recovery switch for several seconds while plugging in USB. Alternatively, the system can set the real time clock persistent bit HW_RTC_PERSISTENT1:0x8005C070:0 and then execute system reboot. Detail can refer to "Boot Modes" section in  reference manual.

Once the MX28 is in recovery mode, PC host can load any MX28 boot stream to the device using sb_loader.exe via USB.

Tags (1)
0 Kudos
Reply
0 Replies