MX27_VPU_FW_2.2.4_UPDATE_TO2.X_ONLY_LINUX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX27_VPU_FW_2.2.4_UPDATE_TO2.X_ONLY_LINUX

Jump to solution
967 Views
weiteyang
Contributor I

hi, i am weite yang,

i are developping a project on i.MX27, to stream audio and video in it . i am going to use Gstreamer to stream  i.MX27's video to PC .

Because i  have no Freescale salesperson /FAE name and email,and i cannot download this package M27_VPU_FW_2.2.4_UPDATE_TO2.X_ONLY_LINUX ,if you have this package,please send me by email : vithome@163.com ,i will  very appreciated. 

Thank you in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
881 Views
Yuri
NXP Employee
NXP Employee

The link for i.MX27 VPU FW is moderated because NDA is needed to get the FW.
So please apply to local Freescale representative for NDA.

View solution in original post

0 Kudos
Reply
1 Reply
882 Views
Yuri
NXP Employee
NXP Employee

The link for i.MX27 VPU FW is moderated because NDA is needed to get the FW.
So please apply to local Freescale representative for NDA.

0 Kudos
Reply