MTD Partition boot parameters being ignored

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MTD Partition boot parameters being ignored

10,521 Views
ajellisuk
Contributor II

Hello

I'm working with Yocto runing on an IMX6 system (MSC Q7iMX6-Plus), and I'm having problems with u-boot-fw-utils not being able to access the u-boot environment variables.

If I type mtdparts in u-boot I see the following output in the console:

U-Boot > mtdparts

device sflash0 <m25p16>, # parts = 4
 #: name                size            offset          mask_flags
 0: init                0x00020000      0x00000000      0
 1: uboot_data          0x00020000      0x00020000      0
 2: uboot               0x00080000      0x00040000      0
 3: boot_logo           0x00140000      0x000c0000      0

active partition: sflash0,0 - (init) 0x00020000 @ 0x00000000

defaults:
mtdids  : none
mtdparts: none

The environment variable for mtdparts in uboot is:

mtdparts=mtdparts=m25p16:0x0000020000@0x0000000000(init),0x0000020000@0x0000020000(uboot_data),0x0000080000@0x0000040000(uboot),0x0000140000@0x00000c0000(boot_logo)

I have confirmed mtdparts is passed in the command line with cat /proc/cmdline

mtdparts=m25p16:0x0000020000@0x0000000000(init),0x0000020000@0x0000020000(uboot_data),0x0000080000@0x0000040000(uboot),0x0000140000@0x00000c0000(boot_logo)

But when I type cat /proc/mtd I see this:

root@msc-q7-imx6plus:~# cat /proc/mtd
dev:    size   erasesize  name
mtd0: 00008000 00008000 "spi0.0"
mtd1: 00008000 00008000 "spi0.1"
mtd2: 00200000 00010000 "spi3.0"

The above output bears no resembalence to the boot parameters or what is shown in u-boot.

After much research into this I'm aware that the mtd partion is setup either in the boot parameters, device tree or in the source itself. I have checked the source code for the device tree for my board, and also the kernel source for the board I'm working with, but cannot find any referenc to mtd partiion table, let alone what is shown by cat /proc/mtd.

So my question is what determines which parameters are used to define the mtd partition table, ie what decides whether it's the command line parameters, device tree, or embedded in the kernel source itself?

Thanks in advance

Andrew

0 Kudos
Reply
3 Replies

10,104 Views
ajellisuk
Contributor II

Hi @igorpadykov  & @[email protected] 

Thank you for your replies.

I have been away from this for a few days, so I've not had a chance to reply sooner.

I believe that I had stumbled accross 2 red herrings. The issue was in the device tree, and the command line parameters were not being used. When I followed the example for creating MTD partitions here, I had added some code which was unnecessary.

The block of code in the device tree originally read:

&ecspi4 {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_ecspi4_1>;
        fsl,spi-num-chipselects = <1>;
        cs-gpios = <&gpio5 2 0>;
        status = "okay";

        flash: spi4@0 {
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "atmel,m25p16";
                spi-max-frequency = <50000000>;
                reg = <0>;
        };
};

Following the example for creating MTD partitions, I ammended the code so it read:

&ecspi4 {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_ecspi4_1>;
        fsl,spi-num-chipselects = <1>;
        cs-gpios = <&gpio5 2 0>;
        status = "okay";

        flash: spi4@0 {
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "atmel,m25p16";
                spi-max-frequency = <50000000>;
                reg = <0>;
//******* Added by Andrew Ellis *********************
                partitions {
                compatible = "fixed-partitions";
                #address-cells = <1>;
                #size-cells = <1>;

                        partition@0 {
                                label = "init";
                                reg = <0x0000000 0x020000>;
                                read-only;
                        };

                        partition@20000 {
                                label = "uboot_data";
                                reg = <0x020000 0x020000>;
                        };

                        partition@40000 {
                                label = "uboot";
                                reg = <0x40000 0x80000>;
                                read-only;
                        };

                        partition@c0000 {
                                label = "boot_logo";
                                reg = <0xc0000 0x140000>;
                        };

                };

                };
//********************************************************************
   };

After reading your replies, and ammending the command line as suggested, I still didn't have any success. I decided to take another look at the device tree, thought I would try removing this block to see what would happen

partitions {
                compatible = "fixed-partitions";
                #address-cells = <1>;
                #size-cells = <1>;
};

And found that the partition table was set up correctly.

The entry in the device tree now reads:

&ecspi4 {
        pinctrl-names = "default";
        pinctrl-0 = <&pinctrl_ecspi4_1>;
        fsl,spi-num-chipselects = <1>;
        cs-gpios = <&gpio5 2 0>;
        status = "okay";

        flash: spi4@0 {
                #address-cells = <1>;
                #size-cells = <1>;
                compatible = "atmel,m25p16";
                spi-max-frequency = <50000000>;
                reg = <0>;

                partition@0 {
                        label = "init";
                        reg = <0x0000000 0x020000>;
                        read-only;
                };

                partition@20000 {
                        label = "uboot_data";
                        reg = <0x020000 0x020000>;
                };

                partition@40000 {
                        label = "uboot";
                        reg = <0x40000 0x80000>;
                        read-only;
                };

                partition@c0000 {
                        label = "boot_logo";
                        reg = <0xc0000 0x140000>;
                };

        };
};

Hopefully this will be some help to anyone else stuggling here.

Best regards

Andrew

0 Kudos
Reply

10,104 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

one can try to debug it in drivers/mtd/cmdlinepart.c

cmdlinepart.c\mtd\drivers - linux-imx - i.MX Linux kernel 

Seems command line parameters can override default.

Best regards
igor

0 Kudos
Reply

10,104 Views
turker
Contributor IV

You need to enable command line mtd partitioning in kernel config. Also I guess Linux is looking for the name of the chip it assigns inside the kernel parameters. So try replacing m25p80 with spi3.0.

mtdparts=mtdparts=spi3.0:0x0000020000@0x0000000000(init),0x0000020000@0x0000020000(uboot_data),0x0000080000@0x0000040000(uboot),0x0000140000@0x00000c0000(boot_logo)

0 Kudos
Reply