MTBF value for PF0100 PMIC and I.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MTBF value for PF0100 PMIC and I.MX6

2,910 Views
aneeshts
Contributor I

Hi All,

   Anybody can provide me Documents that specifies MTBF(Mean Time between failure) or FIT(Failure in time) value for the I.MX6 Quad, Dual,Solo, Dual lite and the PMIC PF0100?




Regards

Aneesh

Labels (4)
0 Kudos
Reply
1 Reply

1,168 Views
igorpadykov
NXP Employee
NXP Employee

He, ANEESH

Freescale does not provide such documents. You

can refer to documents below, for MTBF values you can enter

ticket to Freescale support.

Application Note AN4725 Rev. 0, 05/2013

i.MX 6Solo/6DualLite Product Usage Lifetime Estimates

http://www.freescale.com/files/32bit/doc/app_note/AN4725.pdf

Application Note AN4724 (rev. 0, 04/2013)

"i.MX 6Dual/6Quad Product Usage Lifetime Estimates"

http://www.freescale.com/files/32bit/doc/app_note/AN4724.pdf

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply