Dear supporter
在我们的案子(android4.2.2 upgrade to android 5.0.2)上使用2M camera (Sensor MT9D115)拍照,获得的照片有时会很奇怪:有些画面产生了错乱(请参见附件),复现概率大概有50%
请问有哪些测试分析点可以定位问题的来源?
另外sensor本身应该无问题,因为同一台机器,刷android 4.2的镜像就没有问题,刷android 5.0.2就出现上述问题.
问题很紧急,请帮忙分析一下,给一些debug的方向.
感谢.
- Camera Sensor相关规格 -
• Focusing Type: Fix Focusing
• Frame Rate: SXGA@15fps
• System Interface: Parallel
- 项目平台信息 -
请问您这个问题解决了吗?,我也是用的美光的sensor mt9d112 也是跟你同样的问题
Hello Xingrui,
I can only give you some limited advice, because the camera you are using is not supported by EVK board, I don't have environment to test it.
attachments are 2 patches, you can try to patch them to your system. Remind you had better backup corresponding files before patching.
Regards,
weidong
Dear supporter
With some hardwork, the below config should be set in function vidioc_int_g_ifparm_num()
p->u.bt656.nobt_vs_inv = 1;
could give us more explanation about the rootcause ?