MSI Interrupt not working in Variscite MX6 Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MSI Interrupt not working in Variscite MX6 Board

1,547件の閲覧回数
iqrajaved
Contributor III

Hi all, 

I am working on PCIe driver for Variscite board. I am developing the driver without any OS (linux or other). 

Currently, I/O and MEM read write are working and legacy interrupt is also working. But I am facing problems in MSI. Kindly guide me regarding this. 

The configurations that I have done are: 

1) I have programmed Data register (offset 0x5C) of EP with value 0x0000 and MSI address register (offset 0x54 ) of EP with some address (say 0x01FF8000 as i saw it in the linux pci-e-ep-driver)

2) MSI of EP is enabled by setting MSI_Enable bit of MSI control register (offset 0x52 bit 0)

3) I have configured the RC register MSI controller Address Register (0x01FFC820) with the same address as that of MSI address in EP (i.e., 0x01FF8000). 

4) MSI interrupt #0 enable register (0x01FFC828) is written with the value 0x01 and the Mask register (0x01FFC82C) with value 0

5) The interrupt disable in the RC is set in the command register (0x01FFC004) by setting 10th bit.

6) MSI inbound region # 1 is configured in address match mode by setting following parameters to iATU 

         iATU_ViewPort = 0x80000001;

         iATU_Control1 = 0x0;

         iATU_Control2 = 0x80000000;

         iATU_LowerBaseAddr = 0x01FF8000;

         iATU_UPBaseAddr   = 0;

         iATU_LimitAddr = 0x1FFF;

         iATU_LowerTargetAddr = 0x4F800000; (inbound memory)

         iATU_UpTgtAddr = 0;

After all these configurations I receive no MSI interrupt. Can anyone guide me regarding this strange behavior? 

Thanks.

Iqra Javed

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,209件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  The following may be helpful:

How is iMX6 PCIE endpoint MSI generation setup? 

https://community.nxp.com/thread/321747 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,209件の閲覧回数
iqrajaved
Contributor III

Thank you YuriMuhin_ng‌ for replying. 

I am not working on MSI generation on EP mode PCI, rather I am not able to receive the interrupt in RC mode. 

See if you can help?

Regards,

Iqra Javed

0 件の賞賛
返信

1,209件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  perhaps the following helps.

https://community.nxp.com/docs/DOC-340425 

Regards,

Yuri.

0 件の賞賛
返信