MQS on i.MX6ULL with Linux kernel linux-fslc 4.9.x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQS on i.MX6ULL with Linux kernel linux-fslc 4.9.x

2,104件の閲覧回数
sarelbreet
Contributor I

MQS on i.MX6ULL with Linux kernel linux-fslc 4.9.x

I am trying to get the MQS working on an i.MX6ULL with Linux kernel based on linux-fslc 4.9.x.

Upon kernel start I get an error:

imx-mqs sound-mqs: ASoC: CODEC DAI fsl-mqs-dai not registered

imx-mqs sound-mqs: snd_soc_register_card failed (-517)

 

My kernel debug log is shown below.

Do you maybe have an idea what could be wrong?

 

Thanks in advance for your help.

 

Kind regards,

Sarel

 

----------------------------------------------------------------------------------------------------------------------------

Starting kernel in secure mode

exitcall-> nv_exit+0x0/0x30

exitcall-> devices_shutdown+0x0/0x48

ERROR: imx-usb 2184000.usb: gadget not registered.

exitcall-> arch_shutdown+0x0/0x20

Booting Linux on physical CPU 0x0

Linux version 4.9.75 (sarel@HELIX-AU-SB-DEV) (gcc version 7.3.0 (Buildroot 2018.02.2-g7dd9b6e) ) #27 SMP PREEMPT Wed Nov 7 15:27:17 AWST 2018

CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d

CPU: div instructions available: patching division code

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

OF: fdt:Machine model: Embed smartTouch MK2 EMMC/WIFI-5G

Memory policy: Data cache writealloc

percpu: Embedded 14 pages/cpu @9ffd5000 s25420 r8192 d23732 u57344

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048

Kernel command line: console=ttymxc0,115200n8 root=/dev/mmcblk1p1 rw rootwait noatime consoleblank=0

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 506620K/524288K available (7168K kernel code, 279K rwdata, 2328K rodata, 1024K init, 422K bss, 17668K reserved, 0K cma-reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xa0800000 - 0xff800000   (1520 MB)

    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80800000   (8160 kB)

      .init : 0x80b00000 - 0x80c00000   (1024 kB)

      .data : 0x80c00000 - 0x80c45f60   ( 280 kB)

       .bss : 0x80c47000 - 0x80cb0880   ( 423 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

        Build-time adjustment of leaf fanout to 32.

        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.

RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1

NR_IRQS:16 nr_irqs:16 16

Switching to timer-based delay loop, resolution 333ns

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns

clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)

Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)

CPU: Testing write buffer coherency: ok

/cpus/cpu@0 missing clock-frequency property

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x80100000 - 0x80100058

Brought up 1 CPUs

SMP: Total of 1 processors activated (6.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

OF: Duplicate name in lcdif@021c8000, renamed to "display#1"

VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5

clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

futex hash table entries: 256 (order: 2, 16384 bytes)

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor menu

hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 8 bytes.

imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

mxs-dma 1804000.dma-apbh: initialized

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: can't use DMA, using PIO instead.

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA, using PIO instead.

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.22

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

clocksource: Switched to clocksource mxc_timer1

VFS: Disk quotas dquot_6.6.0

VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NET: Registered protocol family 2

TCP established hash table entries: 4096 (order: 2, 16384 bytes)

TCP bind hash table entries: 4096 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

workingset: timestamp_bits=30 max_order=17 bucket_order=0

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.26)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: Driver registered.

backlight supply power not found, using dummy regulator

21c8000.lcdif supply lcd not found, using dummy regulator

Console: switching to colour frame buffer device 100x30

mxsfb 21c8000.lcdif: initialized

imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2

imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX

console [ttymxc0] enabled

21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 68, base_baud = 5000000) is a IMX

21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 69, base_baud = 5000000) is a IMX

[drm] Initialized

brd: module loaded

loop: module loaded

libphy: Fixed MDIO Bus: probed

CAN device driver interface

2090000.flexcan supply xceiver not found, using dummy regulator

flexcan 2090000.flexcan: device registered (reg_base=a0c20000, irq=26)

20b4000.ethernet supply phy not found, using dummy regulator

pps pps0: new PPS source ptp0

fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00

fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 1a:e8:ff:d6:6c:77

libphy: fec_enet_mii_bus: probed

fec 20b4000.ethernet eth0: registered PHC device 0

2188000.ethernet supply phy not found, using dummy regulator

pps pps1: new PPS source ptp1

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth1: registered PHC device 1

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usb_ehset_test

2184000.usb supply vbus not found, using dummy regulator

ci_hdrc ci_hdrc.0: EHCI Host Controller

ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1

ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

2184200.usb supply vbus not found, using dummy regulator

ci_hdrc ci_hdrc.1: EHCI Host Controller

ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2

ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

random: fast init done

input: EP0790M09 as /devices/platform/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0038/input/input0

i2c /dev entries driver

imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)

Bluetooth: HCI UART driver ver 2.3

Bluetooth: HCI UART protocol H4 registered

Bluetooth: HCI UART protocol LL registered

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

imx-mqs sound-mqs: ==================== imx_mqs_probe =====================

imx-mqs sound-mqs: ----> asrc_pdev

imx-mqs sound-mqs: ASoC: CODEC DAI fsl-mqs-dai not registered

imx-mqs sound-mqs: snd_soc_register_card failed (-517)

NET: Registered protocol family 26

NET: Registered protocol family 10

sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver

NET: Registered protocol family 17

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20161123 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

mmc1: new DDR MMC card at address 0001

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

Registering SWP/SWPB emulation handler

mmcblk1: mmc1:0001 8GME4R 7.28 GiB

mmcblk1boot0: mmc1:0001 8GME4R partition 1 4.00 MiB

imx-mqs sound-mqs: ==================== imx_mqs_probe =====================

mmcblk1boot1: mmc1:0001 8GME4R partition 2 4.00 MiB

imx-mqs sound-mqs: ----> asrc_pdev

mmcblk1rpmb: mmc1:0001 8GME4R partition 3 512 KiB

mmcblk1: p1

imx-mqs sound-mqs: ASoC: CODEC DAI fsl-mqs-dai not registered

imx-mqs sound-mqs: snd_soc_register_card failed (-517)

imx-mqs sound-mqs: ==================== imx_mqs_probe =====================

imx-mqs sound-mqs: ----> asrc_pdev

imx-mqs sound-mqs: ASoC: CODEC DAI fsl-mqs-dai not registered

imx-mqs sound-mqs: snd_soc_register_card failed (-517)

input: keys as /devices/platform/keys/input/input1

imx-mqs sound-mqs: ==================== imx_mqs_probe =====================

hctosys: unable to open rtc device (rtc0)

vdd3p0: disabling

VSD_3V3: disabling

gpio_dvfs: disabling

ALSA device list:

  No soundcards found.

imx-mqs sound-mqs: ----> asrc_pdev

imx-mqs sound-mqs: ASoC: CODEC DAI fsl-mqs-dai not registered

imx-mqs sound-mqs: snd_soc_register_card failed (-517)

EXT4-fs (mmcblk1p1): couldn't mount as ext3 due to feature incompatibilities

EXT4-fs (mmcblk1p1): couldn't mount as ext2 due to feature incompatibilities

EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:1.

devtmpfs: mounted

Freeing unused kernel memory: 1024K

EXT4-fs (mmcblk1p1): re-mounted. Opts: data=ordered

Starting logging: OK

Initializing random number generator... done.

Starting network: OK

 

Welcome to Buildroot

buildroot login: random: crng init done

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,629件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

It seems that you are having some issues in your DTS,  you can check an example :

mqs example can be found in imx6ul-14x14-ddr3-arm2-mqs.dts

linux-2.6-imx.git - Freescale i.MX Linux Tree

documentation: fsl,mqs.txt,imx-audio-mqs.txt

linux-2.6-imx.git - Freescale i.MX Linux Tree

0 件の賞賛
返信

1,629件の閲覧回数
sarelbreet
Contributor I

Thanks for the help. I found that I was missing the CODEC source file sound/soc/codecs/fsl_mqs.c. After adding this, the CODEC is now registered successfully, but when trying to play a sound (simply using speaker-test) it fails as shown below: Thanks for any help. Please note I am a Linux beginner :smileywink:

Starting kernel...

Loading ARM Linux zImage '/mnt/mmc1.0/boot/zImage'
Loading devicetree from '/mnt/mmc1.0/boot/embed-stx-mk2.dtb'
commandline: console=ttymxc0,115200n8 root=/dev/mmcblk1p1 rw rootwait noatime consoleblank=0
Starting kernel in secure mode
exitcall-> nv_exit+0x0/0x30
exitcall-> devices_shutdown+0x0/0x48
ERROR: imx-usb 2184000.usb: gadget not registered.
exitcall-> arch_shutdown+0x0/0x20
Booting Linux on physical CPU 0x0
Linux version 4.9.75 (sarel@HELIX-AU-SB-DEV) (gcc version 7.3.0 (Buildroot 2018.02.2-g7dd9b6e) ) #27 SMP PREEMPT Fri Nov 9 14:30:18 AWST 2018
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
CPU: div instructions available: patching division code
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt:Machine model: Embed smartTouch MK2 EMMC/WIFI-5G
Memory policy: Data cache writealloc
percpu: Embedded 14 pages/cpu @9ffd5000 s25420 r8192 d23732 u57344
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttymxc0,115200n8 root=/dev/mmcblk1p1 rw rootwait noatime consoleblank=0
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 506616K/524288K available (7168K kernel code, 280K rwdata, 2332K rodata, 1024K init, 422K bss, 17672K reserved, 0K cma-reserved, 0K highmem)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xa0800000 - 0xff800000 (1520 MB)
lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80800000 (8160 kB)
.init : 0x80b00000 - 0x80c00000 (1024 kB)
.data : 0x80c00000 - 0x80c46120 ( 281 kB)
.bss : 0x80c48000 - 0x80cb1880 ( 423 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
Build-time adjustment of leaf fanout to 32.
RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80100000 - 0x80100058
Brought up 1 CPUs
SMP: Total of 1 processors activated (6.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
OF: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 256 (order: 2, 16384 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA, using PIO instead.
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
workingset: timestamp_bits=30 max_order=17 bucket_order=0
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
Console: switching to colour frame buffer device 100x30
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
imx-sdma 20ec000.sdma: external firmware not found, using ROM firmware
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 18, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 67, base_baud = 5000000) is a IMX
21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 68, base_baud = 5000000) is a IMX
[drm] Initialized
brd: module loaded
loop: module loaded
libphy: Fixed MDIO Bus: probed
CAN device driver interface
2090000.flexcan supply xceiver not found, using dummy regulator
flexcan 2090000.flexcan: device registered (reg_base=a0c20000, irq=25)
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 20b4000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 22:bc:da:56:11:91
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
2184000.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.0: EHCI Host Controller
ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
random: fast init done
input: EP0790M09 as /devices/platform/soc/2100000.aips-bus/21a4000.i2c/i2c-1/1-0038/input/input0
i2c /dev entries driver
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol LL registered
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
fsl-mqs 2000000.aips-bus:mqs: ------- fsl_mqs_probe --------
imx-mqs sound-mqs: ==================== imx_mqs_probe =====================
imx-mqs sound-mqs: ----> asrc_pdev
imx-mqs sound-mqs: fsl-mqs-dai <-> 2028000.sai mapping ok
imx-mqs sound-mqs: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
imx-mqs sound-mqs: fsl-mqs-dai <-> 2028000.sai mapping ok
NET: Registered protocol family 26
NET: Registered protocol family 10
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
NET: Registered protocol family 17
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
can: broadcast manager protocol (rev 20161123 t)
can: netlink gateway (rev 20130117) max_hops=1
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
mmc1: new DDR MMC card at address 0001
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
mmcblk1: mmc1:0001 8GME4R 7.28 GiB
Bluetooth: BNEP socket layer initialized
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
Bluetooth: HIDP socket layer initialized
mmcblk1boot0: mmc1:0001 8GME4R partition 1 4.00 MiB
8021q: 802.1Q VLAN Support v1.8
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
mmcblk1boot1: mmc1:0001 8GME4R partition 2 4.00 MiB
mmcblk1rpmb: mmc1:0001 8GME4R partition 3 512 KiB
mmcblk1: p1
input: keys as /devices/platform/keys/input/input1
hctosys: unable to open rtc device (rtc0)
vdd3p0: disabling
VSD_3V3: disabling
gpio_dvfs: disabling
ALSA device list:
#0: mqs-audio
EXT4-fs (mmcblk1p1): couldn't mount as ext3 due to feature incompatibilities
EXT4-fs (mmcblk1p1): couldn't mount as ext2 due to feature incompatibilities
EXT4-fs (mmcblk1p1): recovery complete
EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:1.
devtmpfs: mounted
Freeing unused kernel memory: 1024K
EXT4-fs (mmcblk1p1): re-mounted. Opts: data=ordered
Starting logging: OK
Initializing random number generator... urandom start: failed.
done.
Starting network: OK

Welcome to Buildroot
buildroot login: root

# speaker-test

speaker-test 1.1.5

Playback device is default
Stream parameters are 48000Hz, S16_LE, 1 channels
Using 16 octaves of pink noise
Rate set to 48000Hz (requested 48fsl-mqs 2000000.aips-bus:mqs: -----> soc_dai_hw_params
000Hz)
Buffer size range from 64fsl-mqs 2000000.aips-bus:mqs: ---> fsl_mqs_hw_params
to 16384
Period size range fromfsl-mqs 2000000.aips-bus:mqs: -----> soc_dai_hw_params OK
32 to 8192
Using max buffer sizfsl-sai 2028000.sai: -----> soc_dai_hw_params
e 16384
Periods = 4
fsl-sai 2028000.sai: -----> soc_dai_hw_params OK
fsl-sai 2028000.sai: ---------> ASoC: 2028000.sai hw params failed: -22
Unable to set hw params for playback: Invalid argument
Setting of hwparams failed: Invalid argument
#

0 件の賞賛
返信