MQS for imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQS for imx6ul

1,629件の閲覧回数
sankarsalla
Contributor II

Hi All,

Can you please tell me which imx6ul kernel version having mqs driver support ?

Thanks & Regards,

Sankar.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,347件の閲覧回数
sankarsalla
Contributor II

Hi Igor,

With headphones it's working fine...

Thanks @ Regards,

Sankar

0 件の賞賛
返信

1,347件の閲覧回数
sankarsalla
Contributor II

Hi Igor,

Thanks for sharing link.

once loaded the driver,we got logs like below.

# dmesg | grep mqs
[ 2.964898] imx-mqs sound-mqs: fsl-mqs-dai <-> 2028000.sai mapping ok
[ 2.972353] imx-mqs sound-mqs: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
[ 2.979803] imx-mqs sound-mqs: fsl-mqs-dai <-> 2028000.sai mapping ok
[ 3.191163] #0: mqs-audio

We can test with headset or any circuit we have to made?

0 件の賞賛
返信

1,346件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sankar

L4.1.x linux bsps described on below link support mqs (one can check Release Notes included in documentation)

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信