MPU that can support 4x FHD Camera via MIPI-CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPU that can support 4x FHD Camera via MIPI-CSI

Jump to solution
348 Views
andy_kim
Contributor IV

Hello,

 

We are searching for a MPU that support 4x FHD camera through MIPI-CSI interface.

Are there iMX AP series that can support the feature?

 

Thank you.

 

Best regards,

Andy

0 Kudos
Reply
1 Solution
324 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Yes the i.MX95 can handle two 4K with MIPI CSI up to four lanes each. So far there is no other than  i.MX95

Regards

View solution in original post

1 Reply
325 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Yes the i.MX95 can handle two 4K with MIPI CSI up to four lanes each. So far there is no other than  i.MX95

Regards