MPL115A1 Digital barometer with SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL115A1 Digital barometer with SPI

952 Views
amritabrol
Contributor I

I am having problem connecting the barometer to a suitable micro-controller, i don't know which one to use. Also i don't know if i need to program the micro-controller in order to take pressure readings. Can anyone tell me which micro-controller might be compatible or a board that already has a micro-controller and can be used to communicate with the barometer.

I just need to take pressure readings of the MPL115A1.

Tags (1)
0 Kudos
Reply
1 Reply

785 Views
igorpadykov
NXP Employee
NXP Employee

Hi Amrit

please look at APEX board

http://www.nxp.com/products/sensors/pressure-sensors/barometric-pressure-15-to-115-kpa/altitude-pres...

http://www.mouser.com/ds/2/161/AN3956-38659.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply