MPEG2-PS to H.264 transcoding failed with vpuenc_h264 on i.MX8M-mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPEG2-PS to H.264 transcoding failed with vpuenc_h264 on i.MX8M-mini

6,681 Views
Hata-kun
Contributor I

I'm decoding MPEG2-PS file with GStreamer  mpegdec plug-in and encoding it to H.264 

by vpuenc_h264, but error message is generated.

I ran the following pipeline:

GST_DEBUG=3 gst-launch-1.0 filesrc location=./mpeg2.ps  ! mpegpsdemux ! mpeg2dec ! vpuenc_h264 ! filesink location=./dump.h264

I got the following error: 

Setting pipeline to PAUSED ...
====== VPUENC 4 4 4 build on Apr 23 2019 07:42:51. ======
	wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Apr 23 2019 06:54:12)
	vpulib: 1.1.1
	firmware: 1.1.1.65535
0:00:00.064596250 12940	      0x678ef0 WARN	basesrc gstbasesre. c:3583: gst_base_src_start_complete: <filesrcO> pad not activated yet
Pipeline is PREROADING ...
0:00:00.067196750 12940	      0x662a80 FIXME    videodecoder gstvideodecoder. c:933: gst_video_decoder_drain_out: <mpeg2dec0> Sub-class should implement drain() 
0:00:00.067376375 12940	      0x662a80 FIXME    videodecoder gstvideodecoder. c:933: gst_video_decoder_drain_out: <mpeg2dec0> Sub-class should implement drain()
Redistrbute latency...
0:00:00.090570500 12940       0x662a80 WARN     vpuallocator gstvpuallocator. c:125: gst_vpu_copy_phys_mem: TODO: use relevant hardware to accelerate memory copying!
OMX H264 ! HantroHwEncOmx_encoder_create_h264 H264EncInit failed! (-3) openmax_il/source/encoder/encoder_h264.c:772
0:00:00.091269250 12940       0x662a80 ERROR          vpuenc gstvpuenc. c:774:gst_vpu_enc_open_vpu:<vpuenc_h264-0> opening new VPU handle failed: failure
0.00.00.091355000 12940	      0x662a80 ERROR          vpuenc gstvpuenc. c.947:gst_vpu_enc_handle_frame:<vpuenc_h264-0> gst_vpu_enc_open_vpu failed.
0:00:00.091424625 12940	      0x662a80 WARN	mpegpsdemux gstmpegdemux. c.2944: gst_ps_demux_loop:<mpegpsdemuxO> error: Internal data stream error.
0:00:00.091455625 12940	      0x662a80 WARN	mpegpsdemux gstmpegdemux. c.2944: gst_ps_demux_loop:<mpegpsdemuxO> error: streaming stopped, reason error (-5)
ERROR: from element /GstPipeline:pipeline0/GstMpegPSDemux:mpegpsdemux0: Internal data stream error.
Additional debug info:
gstmpegdemux. c(2944): gst_ps_demux_loop (): /GstPipeline:pipeline0/GstMpegPSDemux:mpegpsdemux0:
streaming stopped, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...

MPEG2 PS file is 1920x1080 resolution and 30fps video. Without H.264 encoding, no error occurred.

Could someone advise me ?

If MPEG content needed, it is possible to upload. 

 

0 Kudos
Reply
9 Replies

6,662 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the Table 18. Parser/Demuxer supported audio/video of enclosed file, mpeg2 demux support avi, mpeg2 and mkv, so check if your video is correct format, did you try to other files? the same issue? and how about trying the avidemux to your file?

aiurdemux: aiur universal demuxer plugin supporting
Supports AVI, MKV, MP4, MPEG2, ASF, OGG, FLV, WebM, RMVB

0 Kudos
Reply

6,649 Views
Hata-kun
Contributor I

I tried other content as follows.

MPG container format includes video as MPEG2 video and  audio as MPEG2 Layer-I.

This occurred following error.

root@ucm-imx8m-mini:/opt/tcr# gst-launch-1.0 filesrc location=./sample2_h.mpg  ! mpegpsdemux ! mpeg2dec ! vpuenc_h264 !
filesink location=./dumphoge.h264
Setting pipeline to PAUSED ...
====== VPUENC: 4.4.4 build on Apr 23 2019 07:42:51. ======
        wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Apr 23 2019 06:54:12)
        vpulib: 1.1.1
        firmware: 1.1.1.65535
Pipeline is PREROLLING ...
Redistribute latency...
OMX H264 ! HantroHwEncOmx_encoder_create_h264 H264EncInit failed! (-3) openmax_il/source/encoder/encoder_h264.c:772
ERROR: from element /GstPipeline:pipeline0/GstMpegPSDemux:mpegpsdemux0: Internal data stream error.
Additional debug info:
../../../git/gst/mpegdemux/gstmpegdemux.c(2944): gst_ps_demux_loop (): /GstPipeline:pipeline0/GstMpegPSDemux:mpegpsdemux0:
streaming stopped, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...

However, if encoder plug-in changed from h264 to mpeg2video, no error occurred.

root@ucm-imx8m-mini:/opt/tcr# gst-launch-1.0 filesrc location=./sample2_h.mpg  ! mpegpsdemux ! mpeg2dec ! avenc_mpeg2video ! filesink location=./dumphoge.h264
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Redistribute latency...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock

 Is this content problem ?

0 Kudos
Reply

6,642 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the release note I sent to you, imx8mm vpu doesn't support encoding and decoding mpeg2

0 Kudos
Reply

6,637 Views
Hata-kun
Contributor I

As I can't understand, please show pages in the release note you said.

You mean it is not possible for i.MX8M-mini to do hardware decoding and hardware encoding at same time ?

0 Kudos
Reply

6,608 Views
joanxie
NXP TechSupport
NXP TechSupport

I have already uploaded the release note in the previous reply, could you find it? if yes, you can refer to the

Table 8. Supported features, find the VPU part:

i.MX 8QuadMax and 8QuadXPlus Decoder: HEVC, H.264, MPEG4, MPEG2
i.MX 8M Quad Decoder: HEVC, VP9, H.264, VP8, RV9, AVS, MJPEG, H.263
i.MX 8M Mini Decoder: HEVC, VP9, H.264, VP8
i.MX 8M Mini Encoder: H.264, VP8
i.MX 8M Plus Encoder: 1080p60 HEVC, H.264
i.MX 8M Plus Decoder : 1080p60 HEVC, H.264, VP9, VP8

only imx8qm  and imx8qxp vpu decoder support mpeg2

0 Kudos
Reply

6,594 Views
Hata-kun
Contributor I

We think 'mpeg2dec' plug-in is not vpu based but software based decoder.

The specification of mpeg2dec is as follows.

root@ucm-imx8m-mini:/usr/lib/gstreamer-1.0# gst-inspect-1.0 mpeg2dec
Factory Details:
  Rank                     secondary (128)
  Long-name                mpeg1 and mpeg2 video decoder
  Klass                    Codec/Decoder/Video
  Description              Uses libmpeg2 to decode MPEG video streams
  Author                   Wim Taymans <wim.taymans@chello.be>

Plugin Details:
  Name                     mpeg2dec
  Description              LibMpeg2 decoder
  Filename                 /usr/lib/gstreamer-1.0/libgstmpeg2dec.so
  Version                  1.14.0
  License                  GPL
  Source module            gst-plugins-ugly
  Source release date      2018-03-19
  Binary package           GStreamer Ugly Plug-ins source release
  Origin URL               Unknown package origin

If mpeg2dec is vpu based, why following pipeline results in successful execution ?

gst-launch-1.0 filesrc location=./sample2_h.mpg  ! mpegpsdemux ! mpeg2dec ! fakesink

 

0 Kudos
Reply

6,588 Views
joanxie
NXP TechSupport
NXP TechSupport

sorry for my misunderstanding, I thought you want to encode and decode mpeg2 file by VPU, how about add h264parse after vpuenc_h264?

0 Kudos
Reply

6,583 Views
Hata-kun
Contributor I

No changes occurred.

root@ucm-imx8m-mini:/opt/tcr# root@ucm-imx8m-mini:/opt/tcr# gst-launch-1.0 filesrc location=./mpeg2.ps  ! mpegpsdemux ! mpeg2dec ! vpuenc_h264 ! h264parse ! filesink location=./dumpxx.h264
Setting pipeline to PAUSED ...
====== VPUENC: 4.4.4 build on Apr 23 2019 07:42:51. ======
        wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Apr 23 2019 06:54:12)
        vpulib: 1.1.1
        firmware: 1.1.1.65535
Pipeline is PREROLLING ...
Redistribute latency...
OMX H264 ! HantroHwEncOmx_encoder_create_h264 H264EncInit failed! (-3) openmax_il/source/encoder/encoder_h264.c:772
ERROR: from element /GstPipeline:pipeline0/GstMpegPSDemux:mpegpsdemux0: Internal data stream error.
Additional debug info:
../../../git/gst/mpegdemux/gstmpegdemux.c(2944): gst_ps_demux_loop (): /GstPipeline:pipeline0/GstMpegPSDemux:mpegpsdemux0:
streaming stopped, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
0 Kudos
Reply

6,555 Views
Hata-kun
Contributor I

We had confirmed the problem was resolved by GStreamer 1.16.1 and VPU 4.5.5.

Thank you !

0 Kudos
Reply