MPEG-2 Encoder for i.MX53 utilising the VPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPEG-2 Encoder for i.MX53 utilising the VPU

779 Views
LeonCraven
Contributor II
Hi, Has anyone come across an MPEG-2 encoder that uses the VPU on the i.MX53? The datasheet (IMX53IEC, Page 15, Note 1) states that 70% of MPEG-2 encoding is performed in hardware, however there is no MPEG-2 encoder in the Multimedia Codec package. I've contacted Freescale and they suggested that we contact "third party suppliers", but didn't say who specifically to contact. Freescale's other suggestion was to write the MPEG-2 encoder for the VPU ourselves. Has anyone managed to do this? Regards, Leon Craven
0 Kudos
2 Replies

516 Views
LeonCraven
Contributor II
Every mention of MPEG2 encode is a misprint... the VPU can decode MPEG2.
0 Kudos

517 Views
LeonCraven
Contributor II
After further talks with Freescale, I've found out that the VPU has no MPEG2 encode capability. Every mention of MPEG2 in the datasheets are misprints.
0 Kudos