MPEG-2 Encoder for i.MX53 utilising the VPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPEG-2 Encoder for i.MX53 utilising the VPU

1,518件の閲覧回数
LeonCraven
Contributor II
Hi, Has anyone come across an MPEG-2 encoder that uses the VPU on the i.MX53? The datasheet (IMX53IEC, Page 15, Note 1) states that 70% of MPEG-2 encoding is performed in hardware, however there is no MPEG-2 encoder in the Multimedia Codec package. I've contacted Freescale and they suggested that we contact "third party suppliers", but didn't say who specifically to contact. Freescale's other suggestion was to write the MPEG-2 encoder for the VPU ourselves. Has anyone managed to do this? Regards, Leon Craven
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,255件の閲覧回数
LeonCraven
Contributor II
Every mention of MPEG2 encode is a misprint... the VPU can decode MPEG2.
0 件の賞賛
返信

1,256件の閲覧回数
LeonCraven
Contributor II
After further talks with Freescale, I've found out that the VPU has no MPEG2 encode capability. Every mention of MPEG2 in the datasheets are misprints.
0 件の賞賛
返信