MMPF0200F6AEP for i.mx6SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0200F6AEP for i.mx6SoloX

1,705件の閲覧回数
peralesserrano
Contributor I

hi

is mandatory to use MMPF0200F6AEP for i.mx6sx designs.

This IC still not sold anywhere, and I want to start my design i.mx6sx.

Is there an alternative? I do not want to program MMPF0200.

Should I use discrete components for power?

exists some reference design with components available for i.mx6sx?

ty

ラベル(1)
タグ(1)
0 件の賞賛
7 返答(返信)

1,322件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi perales

it is not mandatory to use MMPF0200F6AEP,

however one needs to provide correct power-up sequence

to processor. In general one can use also discrete components for power,

however I am not aware of example schematcis for that.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,322件の閲覧回数
peralesserrano
Contributor I

hi igorpadykov ty for answer.

MMPF0200F6AEP all have the same sequence on by default, but the levels of voltages are different.

secuen.png

freescale says that all support i.mx6sx, for example MMPF0200F3:

Sin nombre.png

but the levels are not the same:

f.png

can i change MMPF0200F6AEP 0 per MMPF0200F3? is posible?  Ty for answer

0 件の賞賛

1,322件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

only MMPF0200F6AEP supports SX, refer to table


~igorMMPF0200.jpg

0 件の賞賛

1,322件の閲覧回数
peralesserrano
Contributor I

Hi igor

This table says MMP0200F6 is used in the reference design. Others are not used. In the other reference designs MMP0100 is used.

Supported devices are on the table which I have set.

Then you can use for example MMP0200F3 or must be reprogrammed?

0 件の賞賛

1,322件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi perales

This table says MMP0200F6 should be  used for any i.MX6SX

based designs.

You can program NP device also.

0 件の賞賛

1,322件の閲覧回数
peralesserrano
Contributor I

hi igor sorry but I think not

This tablet says MMPF0200F6 is only used in this design (reference desing for i.mx6Sx): SABRE Board Reference Design|Freescale

MMPF0200.jpg

in other reference desing no use MMPF0200, in all use MMPF0100 so the table is empty

Sin nombre.png

SABRE Reference Designs|Freescale

dispositivos.png

sorry for my bad english

0 件の賞賛

1,322件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi perales

if you are novice, it is highly recommended to use

MMPF0200F6 and i.MX6SX Sabre Board as starting

point for first design.

0 件の賞賛