Can the MMPF0100NPEP main input supply voltage (Vin) be less than the switching regulators SW1AIN, SW1BIN, etc?
I would like to use the KITPFPGMEVME Programmer while my board is powered by the programmer (3.3V) or by my board's 4.2V DC/DC converter.
By placing two or-ing diodes from programmer 3.3V and external 4.2V the PMIC can be programmed with system power off or on.
Thank You,
Mark Pascarelli
Solved! Go to Solution.
Hello,
The system VIN is used to supply PMIC core, and there are no restrictions regarding
other voltages.
Regards,
Yuri.
Hello,
Please take into account some minimal voltage drop between input and output voltages
for buck switching regulator.
"What is the minimum VIN voltage to maintain a stable 3.15V on SW2 of the PF0100 PMIC?"
https://community.freescale.com/message/387096#387096
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I am meeting the voltage drops for the input to output requirements.
VIN1 = 3.3V for 1.5V and 1.5V out
VIN2 = 3.3V for 1.8V and 2.5V out
VIN3 = 4.2V for 2.8V and 3.3V out
SW1AIN, SW1BIN, SW1CIN, SW2IN, SW3AIN, SW3BIN, SW4IN, SWBSTIN = 4.2V for 1.375V, 1.375V, 3.3V, 1.35V, 1.2V and 5V outputs respectively.
System VIN (pin 50) = 3.9V
My question is;
Can System VIN be < all other VIN's
Thanks,
Mark
Hello,
The system VIN is used to supply PMIC core, and there are no restrictions regarding
other voltages.
Regards,
Yuri.