MMPF0100 startup with OTP fuses

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 startup with OTP fuses

1,581 Views
joemenard
Contributor I

I'm planning on using the MMPF0100F0AEP which has preprogrammed OTP fuses. I'd like it to start up with the preprogrammed fuse values. With VDDOTP tied to GND will it start up with the preprogrammed fuse values. My confusion is the document states that FUSE_POR_XOR must be set to 1 to start from OTP fuses however I wont be able to program that fuse. Is it already set to 1 in preprogrammed parts? Thank you.

0 Kudos
Reply
2 Replies

1,446 Views
YixingKong
Senior Contributor IV

Joe

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

1,446 Views
joemenard
Contributor I

You can close the discussion. I was told it should start according to the pre-programmed fuses. My board will be here in a couple weeks. If I have issues I'll open a new thread. Thank You.

0 Kudos
Reply