MMPF0100 pin connection when unused.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 pin connection when unused.

ソリューションへジャンプ
1,461件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our partner have some question about MMPF0100 connection when unused.

Please see Table 1 of AN4717 (Schematic Guidelines for the MMPF0100).

[Q1]

The recommended connection when not used for the following pins are "Leave floating".

VGENx

VINREFDDR

VREFDDR

SWxFB

SWxLX

We want to confirm the meaning of "Leave floating".

I understand "Leave floating" means "No Connect", so all circuits and materials written in "Recommended connection" column (e.g. capacitor, shottky diode for SWBSATLS) are NOT required.

Is this correct?

[Q2]

Please see the "Recommended connection when not used" for VINx.

These are written as "Connect to regulator with output voltage < 3.*V", or "Connect to VIN".

I understood these power supplies are required even if all VGEN outputs are unused, we cannot be these pins as "Leave floating".

Is this correct?

Best Regards,

Satoshi Shimoda

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,290件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

1. you are right, all mentioned circuits and materials are NOT required

2. correct

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,291件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

1. you are right, all mentioned circuits and materials are NOT required

2. correct

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信