MMPF0100 pin connection when unused.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MMPF0100 pin connection when unused.

跳至解决方案
1,377 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have some question about MMPF0100 connection when unused.

Please see Table 1 of AN4717 (Schematic Guidelines for the MMPF0100).

[Q1]

The recommended connection when not used for the following pins are "Leave floating".

VGENx

VINREFDDR

VREFDDR

SWxFB

SWxLX

We want to confirm the meaning of "Leave floating".

I understand "Leave floating" means "No Connect", so all circuits and materials written in "Recommended connection" column (e.g. capacitor, shottky diode for SWBSATLS) are NOT required.

Is this correct?

[Q2]

Please see the "Recommended connection when not used" for VINx.

These are written as "Connect to regulator with output voltage < 3.*V", or "Connect to VIN".

I understood these power supplies are required even if all VGEN outputs are unused, we cannot be these pins as "Leave floating".

Is this correct?

Best Regards,

Satoshi Shimoda

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,206 次查看
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

1. you are right, all mentioned circuits and materials are NOT required

2. correct

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,207 次查看
igorpadykov
NXP Employee
NXP Employee

HI Satoshi

1. you are right, all mentioned circuits and materials are NOT required

2. correct

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复