MMPF0100 can satisfy i.MX6DQ ERR007926 POR_B de-assertion timing?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 can satisfy i.MX6DQ ERR007926 POR_B de-assertion timing?

Jump to solution
664 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6DQ ERR007926.

According to errata sheet (IMX6DQCE Rev.5), "Extend the assertion of POR_B until the 32 kHz crystal oscillator is running and stable.".

MMPF0100 can satisfy this condition? or a reset IC is needed?

Best Regards,

Satoshi Shimoda

Labels (3)
Tags (1)
0 Kudos
1 Solution
482 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

MMPF0100 does not check this condition. However crystals may have different

start-up times (time necessary for crystal to become running and stable).

So one needs to choose proper crystal, or add external circuit to satisfy

this condition.

Best regards

igor
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
483 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

MMPF0100 does not check this condition. However crystals may have different

start-up times (time necessary for crystal to become running and stable).

So one needs to choose proper crystal, or add external circuit to satisfy

this condition.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos