Hi Satoshi
when VIN < output setting then regulation transistor will be fully turned on.
So output voltage will follow the input, for example one can refer to
http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
SW2 footnotes 46,47 on p.57 and Figure 18. SW2 Block Diagram:
(VIN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace resistance).
The same is for LDO, one can refer Figure 30. General LDO Block Diagram:
(VIN - VLDO) = ILDO* (RONLDOtransistor + PCB trace resistance).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------