MMPF0100 behavior when VIN is lower than Vout setting.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 behavior when VIN is lower than Vout setting.

ソリューションへジャンプ
1,317件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100.

I want to know the behavior when VIN is under voltage of switching regulators or linear regulators output setting.

(e.g. VIN=3.0V, SW2=3.3V, VGEN3=3.3V)

I understand MMPF0100 goes into coincell mode when VIN < UVDET(2.65V), then how about when UVDET < VIN < Vout?

Vout = VIN in this case? or Vout is stopped?

Best Regards,

Satoshi Shimoda

ラベル(1)
0 件の賞賛
返信
1 解決策
1,174件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

when VIN < output setting then regulation transistor will be fully turned on.

So output voltage will follow the input, for example one can refer to

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

SW2 footnotes 46,47 on p.57 and Figure 18. SW2 Block Diagram:

(VIN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace resistance).

The same is for LDO, one can refer Figure 30. General LDO Block Diagram:

(VIN - VLDO) = ILDO* (RONLDOtransistor + PCB trace resistance).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,175件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

when VIN < output setting then regulation transistor will be fully turned on.

So output voltage will follow the input, for example one can refer to

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

SW2 footnotes 46,47 on p.57 and Figure 18. SW2 Block Diagram:

(VIN - VSW2) = ISW2* (DCR of Inductor +RONSW2P + PCB trace resistance).

The same is for LDO, one can refer Figure 30. General LDO Block Diagram:

(VIN - VLDO) = ILDO* (RONLDOtransistor + PCB trace resistance).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信