MMPF0100 LiCELL charge voltage and i.MX6 RTC operating voltage range

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 LiCELL charge voltage and i.MX6 RTC operating voltage range

ソリューションへジャンプ
1,557件の閲覧回数
george
Senior Contributor II

Dear all,

When connecting rechargeable battery to MMPF0100 and using it as backup for RTC on i.MX6, the charge voltage to battery is 2.5V (default).

=> Page 113 on http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf

That is, battery voltage goes up to 2.5V.

When an external power supply is not connected to a system, RTC needs to work by Battery charged to 2.5V.

However, the operating voltage range of i.MX6 VDD_SNVS_IN is 2.9V-3.3V.

We keep only RTC.

Is really more than 2.9V needed in order to keep RTC?

I think that lower voltage is available in order to keep RTC operation generally.

If it becomes so, since it is necessary to change charge voltage setting to Battery more than 2.9V.

Best Regards,

George

ラベル(1)
0 件の賞賛
返信
1 解決策
892件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

yes it is necessary to change charge MMPF0100 voltage setting to

battery more than 2.9V since IMX6SDLCEC Table 9. Operating Ranges

defines backup battery supply range VDD_SNVS_IN as 2.9-3.3V

Also Table 8 Current Consumption Summary MMPF0100 datasheet :

Typical values are characterized at VIN = 3.6 V, VDDIO = 3.3 V, LICELL = 3.0 V,

VSNVS = 3.0 V and 25 °C, unless otherwise noted.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
893件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi George

yes it is necessary to change charge MMPF0100 voltage setting to

battery more than 2.9V since IMX6SDLCEC Table 9. Operating Ranges

defines backup battery supply range VDD_SNVS_IN as 2.9-3.3V

Also Table 8 Current Consumption Summary MMPF0100 datasheet :

Typical values are characterized at VIN = 3.6 V, VDDIO = 3.3 V, LICELL = 3.0 V,

VSNVS = 3.0 V and 25 °C, unless otherwise noted.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
892件の閲覧回数
george
Senior Contributor II

Dear Igor,

Thanks.

BR

George

0 件の賞賛
返信