MMPF0100: Discrepancy between Dual-lite Sabre and AN4536

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100: Discrepancy between Dual-lite Sabre and AN4536

647 Views
Sebster
Contributor II

Hello Community,

Per AN4536 and datasheet, the F0 variant column identifies a selected voltage of 3.3V on SW2 whereas the SABRE ref design identifies the voltage as 3.0V.   Can you confirm is this MMPF0100 variant default is 3.0V, or has the PMIC used in SABRE Dual-Lite been altered from the F0 pre-programming?

Same oberversation for SABRE Dual-Lite the SW4 output at 1.8V, whereas the datasheet table indicates a voltage of 3.15V for F0. Again this must have been altered right?

Thanks

Seb

Labels (2)
0 Kudos
Reply
1 Reply

528 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sebastien

yes, SW voltages can be changed at run time.

MMPF0100 F0 (preprogrammed)  has SW2 3.3V, SW4 3.15 

Table 10. Start-up Configuration MMPF0100

below part of Sabre SDP, MCIMX6DL-SDP,   SPF-27392  p.19

i.MX6_SABRE_SDP_DESIGNFILES

SPF-27392  p.19.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply