Hello,
From IMX6DQRM Reference Manual rev 3.0 to rev 4.0, tRPA bit in MMDCx_MDCFG1 register is changed
to Reserved with MMDCx_MDCFG1.Reserved[14:12].
In both document, reset value of MMDCx_MDCFG1.tRPA[15] bit seems 1.
But Field Description say that "This read-only field is reserved and always has the value 0."
Is this bit must set to 0?
Or Field Description of this reserved[15:12] is typo and value 0x8 (1000b) is correct?
Best regards,
Ishii.
已解决! 转到解答。
Hello,
As for tRPA parameter in MMDCx_MDCFG1 register:
This parameter is actually a hold over from DDR2 DRAM, which defined 8-bank device Precharge All Allowance
as tRP + 1*tCK. For DDR3, Precharge all need only wait for the tRP time. So this parameter should be set to 'b0
for normal operations.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
As for tRPA parameter in MMDCx_MDCFG1 register:
This parameter is actually a hold over from DDR2 DRAM, which defined 8-bank device Precharge All Allowance
as tRP + 1*tCK. For DDR3, Precharge all need only wait for the tRP time. So this parameter should be set to 'b0
for normal operations.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------