MMDC timing parameter of DDR3 calibration of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMDC timing parameter of DDR3 calibration of i.MX6

Jump to solution
974 Views
Anonymous
Deactivated User

Hi all,

 

I'd like to do DDR3 calibration with i.MX6DL.

Now I'm using MX6DL_SabreSD_DDR3_register_programming_aid_v2.2.xlsx.

 

DDR3 IC itself supports DDR3L-1866, but i.MX6DL supports DDR3-800.

So I have to check the DDR3-800 timing parameter from DDR3 IC's datasheet and set to MMDC timing parameter(DDR device timing parameter) of Register configuration such as tCKE, tRP, tCWL, ...

It's not DDR3L-1866's parameter.

 

Is my understanding correct?

Thanks in advance!

Labels (2)
0 Kudos
Reply
1 Solution
966 Views
Yuri
NXP Employee
NXP Employee

@Anonymous 
Hello,

  I think Your understanding is correct: DDR3-800 based settings should be used

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
967 Views
Yuri
NXP Employee
NXP Employee

@Anonymous 
Hello,

  I think Your understanding is correct: DDR3-800 based settings should be used

Regards,
Yuri.

0 Kudos
Reply
963 Views
Anonymous
Deactivated User

Hi, @Yuri 

 

Thank you for your reply.

I got it!

 

Best Regards,

0 Kudos
Reply