Hi,
i'm working on a i.MX6ULLEVK board, and i'm asked to read an SD card through SPI (SDIO channels are are not available).
I managed to modify the dts and use some of the CSI signals like this :
...
Hi Simone
unfortunately spi mode is not supported by uSDHC module as described in sect.58.8.11 Protocol Control (uSDHCx_PROT_CTRL) in description of D3CD bit i.MX 6ULL Applications Processor Reference Manual
""..card into the SPI mode, which the uSDHC does not support.""
Best regards
igor
Hi Igor,
huge thanks for your quick reply.
Maybe i'm getting that wrong... But, i don't want to use uSDHC module. i'd like to add a new sd device, using SPI1 (or SPI2 it's the same) signals, removed from CSI module. To achieve that, I enabled MMC_OVER_SPI in yocto menuconfing (this is the reference https://www.kernelconfig.io/config_mmc_spi?q=&kernelversion=5.4.118&arch=arm) and i double checked the .config file and all dependecies are imported.
my new device tree is:
&ecspi1 {
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
cs-gpios = <&gpio4 26 0 GPIO_ACTIVE_HIGH>;
status = "okay";
/*
spidev@0x00 {
compatible = "spidev";
spi-max-frequency = <20000000>;
reg = <0>;
};
*/
mmc-slot@0x00 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "mmc-spi-slot";
reg = <0>;
spi-max-frequency = <50000>;
voltage-ranges = <3000 3400>;
disable-wp;
disable-cd;
};
};
It compiles without errors or warnings, and during boot sequence i can see the line:
[ 2.284524] mmc_spi spi0.0: SD/MMC host mmc2, no WP, no poweroff, cd polling
[ 2.289852] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.301530] sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
[ 2.348249] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
[ 2.397736] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
there's the mmc2 instantiated.
Besides, when the os is running, if I insert the sd card in my adapter, i can see these errors:
[ 96.674783] mmc_spi spi0.0: no support for card's volts
[ 96.680106] mmc2: error -22 whilst initialising SD card
[ 96.686496] mmc_spi spi0.0: no support for card's volts
[ 96.697171] mmc2: error -22 whilst initialising MMC card
So i really think that there's a way out....
thanks again
Simone