Dear NXP,
"IMX8M Nano platform"
following error got not able to save while saveenv.
u=> saveenv Saving Environment to MMC... Writing to MMC(2)... MMC: block number 0x2008 exceeds max(0x2000) failed Failed (1)
Hello ,
I'm encoutering the same behaviour on IMX8 board with builded HardKnott Yocto image.
Can you tell me wich emmc partition is checked ? mmcblkXbootY perhaps ?
rgds
Hello Vinothkumars,
The "mmc write" performs raw writes to the MMC device. It does not perform write via the filesystem. There is no "write" support to most of the filesystem access commands. Only ext4 seems to have "write" operation. The "mmc write" you performed probably overwrote the MMC partition table.
This is a bug with this version of U-Boot. Or download the one from yocto file, My suggestion is to use a known stable version of the U-Boot bootloader.
Regards