MLC NAND Support in iMX6UL 4.14.78 kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MLC NAND Support in iMX6UL 4.14.78 kernel

1,918件の閲覧回数
michaelwesley
Contributor I

I'm working on iMX6 UL custom board and it is using NAND flash for booting with the help of 4.1.15 kernel version. UBI filesystem is used to mount the rootfile system. Recently, i moved the kernel version from 4.1.15 to the recent update, 4.14.78 and the board got failed to load the UBI volumes with error report as MLC NAND is not supported.

ubi: refuse attaching mtd12 - MLC NAND is not supported

UBI error: cannot attach mtd12

Why the MLC NAND support is got removed in the new mtd driver? but still the SLC NAND support is available.

I removed the hardware check part from the mtd - ubi support kernel driver file(build.c) and made it work, but still we don't know, why they removed the support. Is it good to go with the patchwork? What kind of issues i can expect? Is there any specific test need to address?

Thanks

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,618件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michael

what bsp used in the case, one can try official nxp release:

Demo Images from

i.MX Software | NXP 

Linux L4.14.78
linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,619件の閲覧回数
michaelwesley
Contributor I

Igor,

We are using the same release(4.14.78) from the code aurora only.

URL :- https://source.codeaurora.org/external/imx/imx-manifest

Branch :- imx-linux-sumo

Manifest :- imx_4.14.78_1.0.0_ga

I attached the error file again and also highlighted the kernel error

report for your reference. Help us, if you get any insight!!!

Thanks

0 件の賞賛
返信

1,619件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michael

one can look on

ubi: Reject MLC NAND - Patchwork 

Best regards
igor

0 件の賞賛
返信