Hi there ,
for testing the i.MX93 , i have ordered the i.MX93 EVK , please someone can recommend me on a MIPI camera and MIPI display , should be plug and play cause its just for the testing.
thanks ,
Leon
Hi , thanks for the response .
i need that the camera will support 1080p with 60 fps , same with the display
and both should connect to the ,MIPI.
dose NXP can offer me such of things ?
Thanks
HI @leonharush,
The CSI MIPI camera module (AP1302 + AR0144) supports a 2-lane configuration and can deliver:
1080p at 45 fps1280×800 at 60 fps
Please note that the display and the camera are connected to separate MIPI ports, so they operate independently.
Best Regards,
Chavira
Hi @leonharush,
Thank you for contacting NXP Support!
Below is the list of compatible accessories for the i.MX93-EVK board:RPI-CAM-MIPI
DY1212W-4856 TFT LCD panel with LVDS interface
IMX-MIPI-HDMI Adaptor Card
MX8-DSI-OLED1A If you have any further questions or need assistance with anything else, feel free to reach out. We're happy to help!Best regards,