MIPI Interface on iMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI Interface on iMX6Q

Jump to solution
2,336 Views
carlosaguero
Contributor II

Hi,

I am trying to configure the iMX6 MIPI interface to use a source that provides MIPI in "non-continuous" clock mode. We have been able to use the iMX6Q with continuous clock mode using OV5640, OV5647, OV5648 video sensors, but now we have a sensor that can't be configured in continuous clock mode.

Question1:

Could somebody please provide information about configuring the iMX6 in non-continuous clock mode for the iMX6?

Currently we found this thread at the community: https://community.freescale.com/thread/341656

Previous link is about a question made to Freescale about the non-continuous clock mode, it states that it is supported but not implemented, also it indicates that there is no documentation on how to configure the iMX6 on non-continuous clock mode.

Question2:

Could you please provide some documentation (if it exists) or hint on how to configure the iMX6 MIPI in non-continuous clock mode?

Question3:

If there is no documentation about MIPI in non-continuous clock mode. Does this means that the iMX6Q MIPI has been used only in continuous clock mode?

Regards and thank you for your time,

Carlos.

Tags (1)
0 Kudos
Reply
1 Solution
1,814 Views
igorpadykov
NXP Employee
NXP Employee

Hi Carlos

latest update from designers:

Non Continuous clock mode is not supported.

There will be added further clarification in the manual that this mode is not supported.

Sorry for confusion.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,814 Views
carlosaguero
Contributor II

Hi,

Thank you very much for the information.

Regards,

Carlos

0 Kudos
Reply
1,815 Views
igorpadykov
NXP Employee
NXP Employee

Hi Carlos

latest update from designers:

Non Continuous clock mode is not supported.

There will be added further clarification in the manual that this mode is not supported.

Sorry for confusion.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply