MIPI DSI to HDMI Audio on i.mx8qxpmek over SPDIF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI to HDMI Audio on i.mx8qxpmek over SPDIF

1,399 Views
rutvij_trivedi
Contributor II

Hi Folks,


I'm using i.mx8qxpmek  and 4.9.51 Distro, I've connected MIPI DSI to HDMI converter having adv7535.
Now my query is its does not seem to have any audio connection provision on i.mx8qxpmek , so i pulled out SPDIF_TX from processor to ADV7535 (MIPI DSI to HDMI Conv.)'s  SPDIF/I2S pin.
SCLK/MCLK and LRCLK are connected with GND at ADV7535 side as from ADV7535 data sheet it says master clock can be ignored.

I've used fsl-imx8mq-evk-dual-display.dts to start HDMI and it works fine with video but how can i get audio working with the above mentioned hardware connection.
I've also gone through AN12188  Rev. 0 , but did not get any clue related to audio.

Requested to en-light me on this.

Thanks & Regards,
Rutvij

Labels (1)
0 Kudos
Reply
2 Replies

1,059 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rutvij

for i.MX8QXP MEK should be used Linux L4.9.88 for i.MX 8QuadXPlus Beta2 as described on

Alpha / Beta BSPs for Microprocessors|NXP 

Support for HDMI audio is described in Release Notes for that package:

pastedImage_2.jpg

Documentation

https://www.nxp.com/docs/en/supporting-information/imx-yocto-L4.9.88_2.2.0-8qxp_beta2.tar.gz 

also on fsl-imx8qxp-mek.dts spdif pins are used as enet :
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/fsl-imx8qxp-...

Seems this support will be added in future linux release.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,059 Views
rutvij_trivedi
Contributor II

Hi, Thanks for the reply.

For HDMI(direct) its okay, i've tested audio even and it worked like charm.
But my query is related to MIPI-DSI TO HDMI Converter using bridgr chip adv7735.



Regards,

0 Kudos
Reply