MIPI DSI communication is not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI communication is not working

760 Views
ajita02
Contributor IV

Hi all,

I am developing display driver over MIPI communication. I driver is getting probed but I am unable to see and data communication between processor and display. Please help, its urgent.

 

> [ 2.458074] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to get blk_ctl
[ 2.479387] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 2.486592] jd9161z_probe 615 Enter jd9161z_probe
[ 2.491308] GrJo: mipi set drvdata
[ 2.494804] GrJo: video mode read
[ 2.495806] imx6q-pcie 33800000.pcie: PCIe PLL locked after 20 us.
[ 2.498124] GrJo: Parsing for reset pin
[ 2.504346] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 2.508164] GrJo:Got panel->reset pin
[ 2.515396] imx6q-pcie 33800000.pcie: IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[ 2.519031] GrJo: reset logic
[ 2.526442] imx6q-pcie 33800000.pcie: MEM 0x18000000..0x1fefffff -> 0x18000000
[ 2.555822] GrJo: GPIO set done
[ 2.558964] GrJo: dev set drvdata
[ 2.562375] GrJo: drm panel added
[ 2.565788] GrJo: rm67191: Exit jd9161z_probe, ret 0
[ 2.570903] imx-drm soc@0:bus@32c00000:display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 2.580982] [drm] Initialized imx-drm 1.0.0 20120507 for soc@0:bus@32c00000:display-subsystem on minor 1
[ 2.590488] GrJo: shine_panel_get_modes
[ 2.594418] GrJo: mode duplicate called
[ 2.598346] GrJo: set mode called
[ 2.601751] GrJo: probe added called
[ 2.605422] GrJo: info set bus format called
[ 2.613329] No hblank data for mode 480x960 with 1 lanes
[ 2.617758] GrJo: Enter rad_panel_prepare()
[ 2.617759] GrJo: Enabling backlight
[ 2.617760] GrJo: After backlight enable
[ 2.643839] GrJo: performing panel reset sequence
[ 2.648988] GrJo: Exit shine_panel_prepare()
[ 2.648991] GrJo: dsi format 0
[ 2.648992] GrJo: Enter shine_panel_enable()
[ 2.648994] GrJo: shine_panel_push_cmd_list()
[ 2.648996] Enter shine_panel_push_cmd_list ...
[ 2.648998] Enter shine_init_sequence ...
[ 3.479850] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[ 3.479854] ret value of read -16 , actual read value 0
[ 3.479856] Exit shine_panel_push_cmd_list normally.
[ 3.479857] GrJo: init sequence completed *********
[ 3.479858] GrJo: Exit shine_panel_enable()
[ 3.497340] No hblank data for mode 480x960 with 1 lanes
[ 3.519622] Console: switching to colour frame buffer device 60x60
[ 3.519732] No hblank data for mode 480x960 with 1 lanes
[ 3.540672] imx6q-pcie 33800000.pcie: Phy link never came up
[ 3.541989] imx-drm soc@0:bus@32c00000:display-subsystem: fb0: imx-drmdrmfb frame buffer device

0 Kudos
5 Replies

637 Views
ajita02
Contributor IV

static const struct drm_display_mode default_mode = {
.clock = 33000,
.hdisplay = 480,
.hsync_start = 480 + 20,
.hsync_end = 480 + 20 + 20,
.htotal = 480 + 20 + 20 + 20,
.vdisplay = 960,
.vsync_start = 960 + 15,
.vsync_end = 960 + 15 + 16,
.vtotal = 960 + 15 + 16 + 4,
.vrefresh = 60,
.width_mm = 23,
.height_mm = 77,
//.bpc = 8,
.type = DRM_MODE_TYPE_DRIVER | DRM_MODE_TYPE_PREFERRED,
};

0 Kudos

638 Views
ajita02
Contributor IV

dts mipi entry ->

&mipi_dsi {
          status = "okay";
  
         panel@0 {
              compatible = "raydium,rm67191";
              reg = <0>;
              pinctrl-0 = <&pinctrl_mipi_dsi_en>;
              reset-gpio = <&gpio1 8 GPIO_ACTIVE_LOW>;
              dsi-lanes = <2>;    // 2 lanes
              video-mode = <2>; /* 0: burst mode
                         * 1: non-burst mode with sync event
                         * 2: non-burst mode with sync pulse
                         */
              panel-width-mm = <23>;
              panel-height-mm = <77>;
             status = "okay";
      };
};

 

0 Kudos

639 Views
ajita02
Contributor IV

I have attached screenshot of my two lane MIPI-DSI. Clock pulses are discontinuous and less (as seen after zooming the screenshot).  My panel is not working. can you please provide me any lead?

SCR05.PNG

0 Kudos

701 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The mipi controller can't receive the dsi packet, maybe you need put some panel configuration before "imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out"

0 Kudos

607 Views
ajita02
Contributor IV

I have attached few details in post. can you help me to give a lead? I am stuck at this from long time.

0 Kudos