MIPI DSI bus turnaround collision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI bus turnaround collision

2,632 Views
emilmyhrman
Contributor IV


Hello,

We're using a MIPI DSI display (controller is ili9488) with imx6dl and are experiencing problems reading registers from the display. After the read command has been sent by imx6 a bus turnaround is also sent, the display then starts to transmit, but it seems as the imx6 then also transmit at the same time, causing a bus contention.

bus turnaround with collision 2.png

Any ideas of what is causing the imx6 to transmit at the same moment as display?

Is there some timeout in imx side causing this? Can the time be extended.

The driver is based on mxcfb_hx8369_wvga.c on Linux 3.14.

Labels (3)
Tags (1)
0 Kudos
Reply
3 Replies

1,806 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You may apply to i.MX6 Platform SDK to check and test

MIPI DSI operations in stand alone environment. Please refer to

Chapter 23 (Configuring the MIPI DSI driver) of "iMX6_Firmware_Guide.pdf"

in SDK documentation.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,806 Views
emilmyhrman
Contributor IV

Hi Yuri,

I can't seem to find the platform sdk anywhere, only thing I could find about it was this post saying it's not supported anymore (https://community.freescale.com/thread/381335​ ).

Regards,

Emil

0 Kudos
Reply

1,806 Views
Yuri
NXP Employee
NXP Employee

You may create request How to submit a new question for NXP Support
or let me know Your e-mail to forward  the SDK.

~Yuri.

0 Kudos
Reply