MIPI DSI LCD display of i.mx8mq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI DSI LCD display of i.mx8mq

3,096 Views
jamesko
Contributor I

Hi,

I am trying to use jdi-lt070me05000(1200x1920 mipi dsi display) on i.mx8mq custom board.

I saw HDMI working fine with DCSS, but now I tried to enable the LCD mentioned above with DCSS(mipi dsi)

Referencing the "fsl-imx8mq-evk-dcss-rm67191.dts" file.

But here I am getting the error as below.

==========================================================================================

[    2.178352] clk: failed to reparent disp_rtrm_pre_div to video_pll1_out: -22

[    2.188997] [drm] Initialized

[    2.197910] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).

[    2.204607] [drm] No driver support for vblank timestamp query.

[    2.210660] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)

[    2.218218] nwl_dsi-imx mipi_dsi@30A00000: Using DCSS as input source

[    2.224976] 30a00000.mipi_dsi_bridge.0 supply power not found, using dummy regulator

[    2.232886] nwl-mipi-dsi 30a00000.mipi_dsi_bridge: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x401

[    2.242789] imx-drm display-subsystem: bound mipi_dsi@30A00000 (ops imx_nwl_dsi_component_ops)

[    2.256144] [drm] OPIPE_CFG: gamut = 1, nl = 1, pr = 1, pix_format = 875713089

[    2.883353] Console: switching to colour frame buffer device 150x120

[    2.945546] imx-drm display-subsystem: fb0:  frame buffer device

==========================================================================================

But, after that, all other prints will look correct, but the LCD will show nothing.

Clock and power sequences are displayed as expected.

fbset command outputs as blow.

Last login: Wed Apr  1 09:01:18 UTC 2020 on tty7

root@myd-imx8mq:~# fbset

 

mode "1200x1920"

    geometry 1200 1920 1200 1920 32

    timings 0 0 0 0 0 0 0

    accel true

    rgba 8/16,8/8,8/0,0/0

endmode

root@myd-imx8mq:~#

 

Please check and provide the correct guide.

 

Thanks in advance,

 

Regards,

Jamesko

Tags (1)
0 Kudos
Reply
7 Replies

2,813 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jamesko

one can try with i.MX8MQ EVK and Demo Images from link

i.MX Software and Development Tools | NXP 

Please verify for correct change the DTB files on Linux:

setenv fdt_file...

saveenv..

Complete procedure is described in Linux Guide from Linux documentation

package on above link:

Linux 5.4.3_1.0.0 Documentation

https://community.nxp.com/docs/DOC-341598 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,813 Views
jamesko
Contributor I

Hi igorpadykov

Thank you for answering first.

A content below the guide are already familiar with and check in several times, and was a modification.

setenv fdt_file fsl-imx8mq-evk-dcss-lt070me05000.dtb

saveenv

reset

It was exactly sure.

I am trying to attach a modified dts file.

Where can I attach it?

Thank you.

Best Regards,

Jamesko

0 Kudos
Reply

2,813 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jamesko

 

what is the reason for modifications of dts file,

one can try with default, follow sect.4. Changing DTS files

on Linux:  "MIPI-DSI-OLED display"

i.MX 8MQ EVK Display Selection Guide 

 

Best regards
igor

0 Kudos
Reply

2,813 Views
jamesko
Contributor I

Hi igorpadykov

The LCD model is different and the manufacturer is different, so we decided to correct it.

Currently supported LCD model : Raydium  RM67191, resolution 1080x1920

LCD model to use : JDI  LT070ME05000, resolution 1200x1920

Thank you.

Best Regards,

Jamesko

0 Kudos
Reply

2,813 Views
igorpadykov
NXP Employee
NXP Employee

for new lcd its specific initialization (based on its datasheet) should be added in driver source

cmd_set_entry manufacturer_cmd_set[], struct drm_display_mode default_mode, rad_panel_enable()

panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel 

Best regards
igor

0 Kudos
Reply

2,813 Views
jamesko
Contributor I

Hi igorpadykov,

I used the driver in the kernel.

panel-jdi-lt070me05000.c\panel\drm\gpu\drivers-linux-imx-i.MX linux kernel

Are there any problems with this driver?

Thank you.

Beat regards,

Jamesko

0 Kudos
Reply

2,813 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jamesko

>Are there any problems with this driver?

probably not if you also correctly configured .dts file.

Best regards
igor

0 Kudos
Reply