MIPI Cameras on i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI Cameras on i.MX6Q

807 Views
hareeshdas
Contributor II

  In i.MX6q based board, Is it also possible to get the sensor data from a 2 lane camera if we configure the MIPI CSI2 as a 4 lane inerface. ( Here I want to use both 4 lane camera and 2 lane camera at the same platform ).

Thanks,

Hareesh

Labels (2)
0 Kudos
Reply
1 Reply

546 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hareesh

I am afraid not, since MIPI-CSI 2 will expect valid data on all 4 lanes

and receive data will fail due to crc check.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------