Hi
We are using Freescale SabreSDP demo board to test it.
My Uboot setting is 1920x1080M@60 HDMI outout only.
We had test half fps issue in Yocto 3.14.28_1.0.1patch when we set mipi camera is 1920x1080 30 fps preview.
It don't happen in Yocto 3.10.53
My command is
gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw, format=(string)NV12, width=1920, height=1080, framerate=(fraction)30/1' ! queue ! imxv4l2sink -v
3_10_53 log
^Chandling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:00:14.391323002
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total showed frames (427), playing for (0:00:14.853627335), fps (28.747).
Freeing pipeline ...
root@imx6qsabresd:~#
3.14.28 log
^Chandling interrupt.
Interrupt: Stopping pipeline ...
EOS on shutdown enabled -- Forcing EOS on the pipeline
Waiting for EOS...
Got EOS from element "pipeline0".
EOS received - stopping pipeline...
Execution ended after 0:00:08.907332001
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total showed frames (108), playing for (0:00:08.908042334), fps (12.124).
Freeing pipeline ...
more detail log , you can see attached file.
Original Attachment has been moved to: 3_14_28_capturelog.txt.zip
Original Attachment has been moved to: 3_10_53_capturelog.txt.zip
Solved! Go to Solution.
Hi Apollo,
Can you try with the next pipeline?
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! video/x-raw,width=1920,height=1080 ! autovideosink
I tried it out and it seems to be working.
/Alejandro
Hi,
I just tried the next :
gst-launch-1.0 imxv4l2src device=/dev/video1 ! 'video/x-raw, format=(string)NV12, framerate=(fraction)30/1' ! queue ! imxv4l2sink -v
and I got the below output uisng 3.14.28
handling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:00:18.172176669
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total showed frames (469), playing for (0:00:18.177413336), fps (25.801).
Freeing pipeline ...
I just removed the height and width of the pipeline.
Best Regards,
Alejandro
Hi alejandrolozano,
If removed the height and width of the pipeline ,I will see default height is 640 , width is 480.
We need to test 1920x1080 30 fps MIPI camera input and output to 1080p60 HDMI.
We also using 3.14.28 mxc_v4l2_overlay function to test this function , it don't has fps lost.
./mxc_v4l2_overlay.out -di /dev/video1 -iw 1920 -ih 1080 -ow 1920 -oh 1080 -fr 60 -m 5 -r 0 -fg -t 100
It seem gstream1.0 issue.
Hi Apollo,
Can you try with the next pipeline?
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! video/x-raw,width=1920,height=1080 ! autovideosink
I tried it out and it seems to be working.
/Alejandro
Hi alejandrolozano,
This command can work..
gst-launch-1.0 -v imxv4l2src device=/dev/video1 ! video/x-raw,width=1920,height=1080 ! autovideosink
Thanks ...
Apollo Chang