MIPI CSI Line Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIPI CSI Line Interrupt

跳至解决方案
1,899 次查看
t-sugiyama
Contributor III

Hello,

I have a question about the LINE_END interrupt of the MIPI CSI of i.MX8Mmini.
I set LINE_INTR of "Line Interrupt Ratio" to 0x1.
In this case, when is the LINE_END interrupt timing of "Interrupt source register 1"?
Is the size of the received data relevant?

Thanks.

Tetsuya.

标记 (1)
0 项奖励
回复
1 解答
1,742 次查看
art
NXP Employee
NXP Employee

With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.

Best Regards,
Artur

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,743 次查看
art
NXP Employee
NXP Employee

With this setting, the LINE_END interrupt will be raised each time the Line End packet is detected on a specific MIPI CSI lane.

Best Regards,
Artur

0 项奖励
回复