MIMXRT1176 MAC address in fuse bits default value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1176 MAC address in fuse bits default value

750 Views
wlan
Contributor III

What are the expected values of the MAC address fuse bits Fuse 0xA80 (MAC1_ADDR), 0xAA0 (MAC2_ADDR), 0xAC0 (MAC3_ADDR) in the RT1176?

On my current device reading the fuses from software via OCOTP and from the MCUXpresso Secure Provisioning tool returns all zeros but I remember that on another board with the same processor, the values were populated.

Are they zero by default or should they hold a "valid" unique MAC address? I did not find that information in the reference manual.

Thanks

0 Kudos
Reply
0 Replies