MIMXRT1176 Flexspi1 Hyper flash with eMMC device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1176 Flexspi1 Hyper flash with eMMC device.

1,281 Views
kitsohn
Contributor I

Hi,

I need help for my system operation configuration.

In my design, USHDC1 as wifi module interface dedicated, and Flexspi1 as Hyperflash boot device.

My question is that is it possible to connect eMMC ic on Flexspi1 interface directly used as USHDC2 interface after boot operation ?

By system usage, wifi and eMMC will operate simultaneously, so the eMMC does not connected to USHDC1 as like EVM board configuration.

kitsohn_0-1667704875006.png

 

Pls advice to me or other way to add eMMC device.

Thanks in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,264 Views
jeremyzhou
NXP Employee
NXP Employee


Hi @kitsohn ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The proposal is not feasible if the code is executed in the HyperFlash, so you should choose other pins to connect Hyper Flash or the Wifi module, in another word, they can't share the same pins.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

0 Kudos
Reply

1,262 Views
kitsohn
Contributor I

Thanks for your timely manner, jeremyzhou.

How about if the code is executed in the external RAM device (SEM interface) not the Hyper flash.

 ; At the start of boot codes, the FW paskage codes will be copied to RAM and executed in RAM.

I know that my design architecture was not recommend, but other ways noting.

Pls consider it and advise to me.

Thanks.

 

 

0 Kudos
Reply

1,258 Views
jeremyzhou
NXP Employee
NXP Employee


Hi @kitsohn ,
Thanks for your reply.
1)How about if the code is executed in the external RAM device (SIM interface) not the Hyper flash.
-- It's available to make it under this case.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the

0 Kudos
Reply