Hi,
All demos for the 1170EVK appear to use the QuadSPI flash for code. Are there any examples that use the OctalSPI flash device instead for XiP? Specifically all examples include an SDK driver file named 'evkmimxrt1170_flexspi_nor_config.c' which is the FlexSPI Configuration Block definition for the QuadSPI. Is there a version of this file anywhere that is configured for the OctalSPI device (MX25UM51345G)?
I looked at generating it myself but the 1170 reference manual is scant on information regarding how exactly to configure some if the parameters in the FlexSPI Configuration Block.