MIMXRT106S processor is not available in keil and in MCUXpresso config tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT106S processor is not available in keil and in MCUXpresso config tool

Jump to solution
2,299 Views
nikint
Contributor I

Hi,

We had selected MIMXRT106SDVL6B processor for our product development. We are using Keil IDE for development and generate code from MCUXpresso Config tool. But when we were creating new project, we did not find processor we selected in IDE. IDE's has MIMXRT1061xxx6A series available. 
So our queries are -

1. Can we use MIMXRT1061xxx6A series processor for project creation?

2. If we select MIMXRT1061xxx6A series processor, does it impact during code flashing?

3. Do we need to download package for MIMXRT106SDVL6B processor?

Thank you.

0 Kudos
Reply
1 Solution
2,291 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @nikint 

  Please check the RT106S SDK, you can find it didn't support the MDK:

kerryzhou_0-1644212242320.png

That's why you can't find the keil project.

 So, to the easy get start, I highly suggest you use the MCUXPresso IDE, which is free and easy to use.

Then, even you use the related driver, you can use the SDK code directly.

https://mcuxpresso.nxp.com/en/builder?hw=SLN-LOCAL2-IOT

 But, if you just want to use the RT1060, no local detect function in the SDK, then you can use the RT1062 chip as the partnumber.

 

Wish it helps you!

Best Regards,

Kerry

 

View solution in original post

3 Replies
2,103 Views
subodh1978
Contributor I

Dear Nikit,

We are also facing the same Problem.

Have you solved this problem ?

I will be very thankful if you share the solution of the same.

Regards

Subodh

 

0 Kudos
Reply
2,292 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @nikint 

  Please check the RT106S SDK, you can find it didn't support the MDK:

kerryzhou_0-1644212242320.png

That's why you can't find the keil project.

 So, to the easy get start, I highly suggest you use the MCUXPresso IDE, which is free and easy to use.

Then, even you use the related driver, you can use the SDK code directly.

https://mcuxpresso.nxp.com/en/builder?hw=SLN-LOCAL2-IOT

 But, if you just want to use the RT1060, no local detect function in the SDK, then you can use the RT1062 chip as the partnumber.

 

Wish it helps you!

Best Regards,

Kerry

 

2,088 Views
subodh1978
Contributor I

Dear Sir,

We have made a PCB using MIMXRT106SDVL6B.

Please find attached Schematic of the same.

We are using MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13] and MCU LINK PRO to load program in the same.

But we are unable to detect the device.

We have tried selecting device 1062xxxxB and 106SxxxxA , But we get Cannot connect to target.

Please find attached screenshot of the same.

Please Let us know, If we have made any mistake !

Regards 

unable to connect.jpg

Subodh

0 Kudos
Reply