MIMXRT106S processor is not available in keil and in MCUXpresso config tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIMXRT106S processor is not available in keil and in MCUXpresso config tool

跳至解决方案
2,562 次查看
nikint
Contributor I

Hi,

We had selected MIMXRT106SDVL6B processor for our product development. We are using Keil IDE for development and generate code from MCUXpresso Config tool. But when we were creating new project, we did not find processor we selected in IDE. IDE's has MIMXRT1061xxx6A series available. 
So our queries are -

1. Can we use MIMXRT1061xxx6A series processor for project creation?

2. If we select MIMXRT1061xxx6A series processor, does it impact during code flashing?

3. Do we need to download package for MIMXRT106SDVL6B processor?

Thank you.

0 项奖励
回复
1 解答
2,554 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @nikint 

  Please check the RT106S SDK, you can find it didn't support the MDK:

kerryzhou_0-1644212242320.png

That's why you can't find the keil project.

 So, to the easy get start, I highly suggest you use the MCUXPresso IDE, which is free and easy to use.

Then, even you use the related driver, you can use the SDK code directly.

https://mcuxpresso.nxp.com/en/builder?hw=SLN-LOCAL2-IOT

 But, if you just want to use the RT1060, no local detect function in the SDK, then you can use the RT1062 chip as the partnumber.

 

Wish it helps you!

Best Regards,

Kerry

 

在原帖中查看解决方案

3 回复数
2,366 次查看
subodh1978
Contributor I

Dear Nikit,

We are also facing the same Problem.

Have you solved this problem ?

I will be very thankful if you share the solution of the same.

Regards

Subodh

 

0 项奖励
回复
2,555 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @nikint 

  Please check the RT106S SDK, you can find it didn't support the MDK:

kerryzhou_0-1644212242320.png

That's why you can't find the keil project.

 So, to the easy get start, I highly suggest you use the MCUXPresso IDE, which is free and easy to use.

Then, even you use the related driver, you can use the SDK code directly.

https://mcuxpresso.nxp.com/en/builder?hw=SLN-LOCAL2-IOT

 But, if you just want to use the RT1060, no local detect function in the SDK, then you can use the RT1062 chip as the partnumber.

 

Wish it helps you!

Best Regards,

Kerry

 

2,351 次查看
subodh1978
Contributor I

Dear Sir,

We have made a PCB using MIMXRT106SDVL6B.

Please find attached Schematic of the same.

We are using MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13] and MCU LINK PRO to load program in the same.

But we are unable to detect the device.

We have tried selecting device 1062xxxxB and 106SxxxxA , But we get Cannot connect to target.

Please find attached screenshot of the same.

Please Let us know, If we have made any mistake !

Regards 

unable to connect.jpg

Subodh

0 项奖励
回复