Hello,
I had build a board wich include MIMXRT1064DVL6A. After burning BT_FUSE_SEL to '1' (have not the boot pin) with NXP-MCUBootUtility bu USB, I succeed in programming the IMXR1064 in the flash (BOOT_MODE not connected).
On new PCB board, the designer put by mistake another reference MIMXRT106ADVL6B instead of MIMXRT1064DVL6A.
I did not succeed to program my board with the106A.
My questions are
1) What is difference between MIMXRT1064DVL6A and MIMXRT1064DVL6B?
2) Can I program MIMXRT106ADVL6B (internal flash), I have not external flash and no possibility to put it?
I succeed in burnning BT_FUSE_SEL to '1', by connected to LSPI NOR/EEPROM first but not programming with the106A.
Is there the only possibility to put MIMXRT1064DVL6A or MIMXRT1064DVL6B to make it work.
Thank you for your help,
Best regards,
Patrice