MIMXRT1052 burned down?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1052 burned down?

698件の閲覧回数
alex5577
Contributor I

The chip on the debug Board EVK-MIMXRT1050 burned down after I left it enabled with the example (..\MCUXpressoIDE_10.2.0_759\workspace\evkbimxrt1050_igpio_led_output) running. I'm using the SDK version 2.4.0 package for EVKB-IMXRT1050 board! Has anyone had similar problems or I was so lucky?

0 件の賞賛
返信
1 返信

555件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Alex,

I dont think it burned, but I will run the test.

You can ask for a replace in the Returns and Warranty Information|NXP 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信