MIMXRT1050-EVK : supply with external 3.3 V ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1050-EVK : supply with external 3.3 V ?

597 Views
manuardi
Contributor II

hi all,

Is it possible to supply the MIMXRT1050-EVK with an external 3.3 V supply ? ( so NOT with 5v/J2 connector). If yes, how ?

Thank's in advance for your reply !

0 Kudos
Reply
1 Reply

477 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Manu,

In case of the i.MX RT1050 EVK, all the supply options (J2, J9 or J28) are 5V inputs. However, the device itself could be powered with single 3.3V using the internal DC-DC (if not using USB). For additional details, you could refer to application note AN12051 “Migration Guide from i.MX6UL to i.MXRT”, especially on section 3.1 “Power Supply”.

Hope this will be useful for you.

Best regards!

/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------