MIMXRT1024 Linux DTS for GPIO interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIMXRT1024 Linux DTS for GPIO interrupt

跳至解决方案
1,615 次查看
sbabu
Contributor III

Hi All,

I want to use GPIO_SD_B1_05 to 08 (GPIO port 3 ) as interrupts which will trigger a interrupt on raising edge on MIMXRT1024 running Linux. Can anybody please share any reference DTS file to achieve the same. Do I need to make any other changes in driver etc other than the DTS entry. Thanks in advance.

Regards,

Babu

 

 

 

标签 (2)
0 项奖励
回复
1 解答
1,586 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sbabu ,

  Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.

  Or your use the linux gcc to compile the RT1024 code?

   Until now, we still don't have the linux DTS for the RT1024.

 

Wish it helps you!

Best Regards,

Kerry

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,587 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sbabu ,

  Do you mean, your RT1024 code is based on linux os? RT1024 can't support the linux, it can use the freertos.

  Or your use the linux gcc to compile the RT1024 code?

   Until now, we still don't have the linux DTS for the RT1024.

 

Wish it helps you!

Best Regards,

Kerry

0 项奖励
回复
1,580 次查看
sbabu
Contributor III

Hi 

@kerryzhou - Thanks. No worries. We will check on it.

0 项奖励
回复