Hi we are in the middle of bringu=ing up an iMX8dl based design. the eth0 is routed to an NXP eth switch.
but we only see a 25MHz clock expecting a 50mHz.
attached the schematic section for the imx and the switch.
Question: please confirm if the connectiones between imx and SJA1110 are done properly for RGMII interface or MII interface.
Also please confirm what speeds are supported as the DS only talks about 100Mbps (RGMII) or 100Mbps (RMII) but the RM menatioans all :
14.5.2.2 Using PHY interfaces
This module support the following modes:
• RMII 10/100 Mbps interface
• MII 10/100 Mbps interface
• RGMII 10/100/1000 Mbps interface
Br Martijn