MIMX8MM5CVTKZAA芯片温度高

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMX8MM5CVTKZAA芯片温度高

815 Views
george_li
Contributor I

请帮忙确认MIMX8MM5CVTKZAA在功耗相当的情况下,比IMX8MM6DVTLZAA芯片表面温度高很多的原因是什么?

底板                                                                                                                                                  核心温度

demo

不插u盘、以太正常工作

自产的核心板(电源芯片BD71837)、原版demo程序

5v/2A

228ma

58(10min)

demo

不插u盘、以太正常工作

原版的核心板(电源芯片BD71837)、原版demo程序

5v/2A

241ma

43(10min)

demo

不插u盘、以太正常工作

原版的核心板2(电源芯片PCA9450)、配套程序

5v/2A

258ma

54(10min)

 

demo

不插u盘、以太正常工作

更好了CPU,自产的核心板(电源芯片BD71837)、原版demo程序

5v/2A

243ma

45(10min)

 

Labels (1)
Tags (1)
0 Kudos
1 Reply

747 Views
b36401
NXP Employee
NXP Employee

Please note that MIMX8MM5CVTKZAA is industrial part and MIMX8MM6DVTLZAA is consumer one. It may take some small difference in temperature.

Also please note that maximal frequency for MIMX8MM5CVTKZAA is 1.6 GHz and 1.8 GHz for MIMX8MM6DVTLZAA. So there may be some difference at low frequency.

0 Kudos